Hello,
I guess this is a very stupid question.
I have been very confused with the Battery Capacity (min) in the search engine, does this value represent the minimal capacity of the battery that I used? Or does it mean that my battery cannot be gauged when its capacity drops below this value? For example, if I want to find a proper gauge ic for a 150mAh LiPo battery, can I use one with 100mAh minimal battery capacity? Would it stop gauging when my battery is depleted below 100mAh?
Many thanks,