Hi. I have noticed that FC flag is set when the battery is not really fully charged.
I want my battery to stop charging when its voltage is 16,8V and current has dropped to 1A. So the parameters of the gauge are : taper voltage - 250mV, taper current - 1A, taper capacity - 5 mAmphr
What I noticed is that the Fc flag is set when voltage of battery is 16624mV, current is 1,6A and the capacity change in last 2 cycles(40sec x 2) is 9mAh. So I guess the Fc flag is not set by these taper parameters.
Questions:
1. Does taper termination occurs if all 3 A, B and C occurs or it needs only one of them to set Fc flag? Picture below:
2. How can I know which of these 3 (taper, delta temperature, negative delta voltage) ways sets the Fc flag?
3. How can I disable the delta temperature and negative delta voltage so it does not set the FC flag?
Thanks in advance.
Karlis