Other Parts Discussed in Thread: BQ21040, BQ25504, BQSTUDIO, CC2650, BQ27441-G1
I am using the BQ27441 gauge IC to calculate a 1320mAh LiOn battery remain capacity and state of charge.
Those values are not correct.
I have the BQ25504 nano power that gets power from a solar panel and puts in to the battery and also have a USB charger BQ21040 that can charge up to 800 mAh on fast current mode.
What would be my Taper Rate and my Taper Current in this case?
So far as i understood it, the taper current is the input current from the charger once it consider battery full right?
or is it 0.1* current charge from the BQ25504/BQ21040?
Does the gauge trace still works if i use both charging system?