This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27531-G1: Bq27531 program df.fs fail

Part Number: BQ27531-G1
Other Parts Discussed in Thread: BQ27531EVM, BQEVSW, BQSTUDIO

Dear all:
         I face a issue which can't re-program Bq27531EVM and my steps as below.

1. Use bqEVSW to program .senc default file and the resault is successful.
2. Use Bqstudio software to program customer's df.fs file. After this step that I can't re-program, it seems Bq27531 latch.

Althought change I2C address 0x16 or 0xaa via bqEVSW software, I read data at "Read I2C Data Block" and show error code=772.

May I have a solution to un-latch Bq27531?

Thanks!