BQSTUDIO - I want to either disable autodetect, or switch between connected devices easily
I have both a TI Power Management device bq25895M, and a fuel Gauge, bq27742-1, working and sharing the I2C bus in a new design.
To switch between them in bqStudio, I must relaunch BqStudio with the usb disconnected. This blocks the auto-detect, and then I re-plug the USB after manually selecting the target device.
Questions:
1) Is there an easy way to switch between target devices, once bqstudio is running
2) Is there a way to disable auto-detect in bqstudio launch?
Most gratefully,
Michael B