Hi,
I have configured the BTP Function on the alternative LED Pin 12 as I have currently used Pin 14 for the Precharge FET.
Settings:
BTP_EN = 1
BTP_POL = 0
LED3BTPALT = 1 (As I want to use Pin 12 as BTP Output)
PCHGBTP = 0 (As I want to use Pin 14 for the Precharge FET)
Init Discharge SET = 300mAh
Init Charge Set = 1000mAh (I set this higher than the capacity as I do not want an BTP event during charging, only if the remaining capacity during discharge drops below 300mAh.)
Whatever I do, the BTP Pin 12 remains LOW.
Also, the BTP_INT status in Operation Status A remains always set (red).
Please explain what I have to do to get this feature working.
Thanks,
Fred