Other Parts Discussed in Thread: BQ20Z80
Hello,
in the TRM of bq40z50-r1 under chapter 4.6 "Valid Charge Termination" it says that if a valid charge termination happens, BatteryStatus[TCA] and GaugingStatus[TCA] will be set to 1 if SOCFlagConfig B[TCASETVCT] = 1. However the register reference for SOC Flag Config B or SOC Flag Config A (chapter 4.2.1.8) does not show any TCASETVCT bit. Also in Battery Management Studio I can't find TCASETVCT in the flag config registers. Is the setting available or not?
I'm asking, because the old bq20z80 set the TCA bit if a valid charge termination happened and the bq40z50-r1 seems not to do this. Our charging station however uses this bit among others to detect end of charging and we would like to keep it compatible to both BQs.
Thanks,
Sebastian