Other Parts Discussed in Thread: BQSTUDIO
Hi,
I use a bq40z60 in a 2-cell 4100 mAh (2050 mAh/cell) Li-Po in a new custom design. My final goal is to charge it from 12V (car battery voltage) or from 24V (truck battery voltage).
- Introduction :
I had a previous design for test purpose that worked fine with both 12V and 24V input on VAC.
We needed to reduce PCB size a lot (0402 cap/resistors, etc) and integrate other parts of the system (MCU, voltage regulators, etc) on the same PCB.
I used the .srec from previous device to put in in new design.
- Problem origin :
At first, voltage and current measurement were OK with 12V charging. But when I wanted to charge it with 24V, the chip became hot (up to 55°C from bqStudio DashBoard) while on the previous design it didn't go much than 40°C.
- Mistake :
I tried to do a learning cycle (discharge) with about 300 mA load, but I forgot to disable computer auto-shutdown and I couldn't do a complete cycle. When I restrat system, current measurement was wrong (about 20mA difference from my HAMEG HM7044 supply and bqStudio) so I tried to do a current calibration :
1) I applied 12V supply on VAC, current measurement on the power supply was 300 mA (decreasing a bit while battery was charging).
2) I then entered 300 mA in current calibration and applied Gas Gauge Calibration.
3) Instantaneously, current on bqStudio and power supply where OK, but when I changed voltage to 11V, current on supply was about 450 mA while it was only 320 mA on bqStudio.
Since that current measurement is wrong even if I program it with original .srec, and it always heat up at 24V...
Is it possible to place the device in full factory settings (calibration too) ?
Thank you.
Regards,
Loic