Other Parts Discussed in Thread: BQSTUDIO
Fellow community members,
I am having an issue with seeing a valid Primary Charge Termination using the bq40z50-R1. I have a charger that we have developed for the bq20z series that I am trying to extend to the bq40z50-R1. My charger shuts down and signals 100% charge when RSOC=100%. The pack firmware is configured such that RSOC stays at 99% until Primary Charge Termination. I have checked the conditions for PCT and believe I am meeting them, but it never goes to PCT. Interestingly enough, when I remove the battery from the charger and then re-connect it, it signals >95% RSOC (a condition programmed into the charger and identified by reading RSOC) for about 5 seconds and then gets the 100% RSOC which switches it to giving a fully charged signal. One of the problems I am having with monitoring this situation is that I cannot use both the smart charger and the bqStudio at the same time. If I do, the charger appears to function properly, but the bqStudio will not communicate. Can anybody help me with either or both of these issues?
Regards,
George W. Mortimer, PE