Other Parts Discussed in Thread: BQ34Z100
Hi,
I have an 8s2p LiFePO4 battery with a BQ34z100-g1. I ran the learning cycle and obtained the golden image, loaded this golden image in every BQ34z100-g1 and installed in the application.
However I have having a problem with SoC estimates because it appears to works fine until suddenly it falls to 0%. At first moment I though it was debt to power loss but I have check it and this occurs althouh no power loss happened.
I have logged it and attach the file. The log starts with the battery full and a motor discharge it in no continuos periods. SoC_Error_GL.log
1. Why do SoC falls to 0%?
2. What can be happening?
If you need more data you only have to ask for it. I can log the real application esaily.
Thankyou,