Part Number: bq20z95
I have to read the whole GG flash from my test program, and it works for the most part, except for reading the Calibration class, Data subclass 104.
I can read the subclass/page in my C code, but when I try to parse into subclass parameters, I get mostly garbage:
The raw data from my 33 byte read from subclass 104 is 0x 15 81 6E D9 06 94 07 E0 BA 5F 82 05 08 56 22 F8 00 00 74 27 FA 00 B1 B1 B1 B1 B1 B1 B1 B1 B1 B1 B1 00.
(I always read 1+32 bytes at a time when I read the data flash, but that should not affect the data. my buffer is big enough to keep the data.).
I wonder if the information in the "bq20z90-V1.50 + bq29330, bq20z95 Technical Reference" (pages 194, 210) is incomplete/inaccurate?
The rest of the data flash comes out OK.
Thank you.