Other Parts Discussed in Thread: BQSTUDIO,
Hello,
I started learning (TI_enabled) but then procedure was interrupted - battery power disconnected, bqStudio shut down, etc, I now cannot change/update info or re-calibrate? I also note that the voltage and current do not always read correctly, especially when bq34z100 is shut down; I need to re-calibrate?!
There is option to enable TI, but none to disable; what needs to be done so I can change/update data info?
What is the procedure from this point to start a new learning cycle on a 12V, 100Ahr(10hr)/66.2Ahr(1hr) Battery? I need to see that SOC follows PbA Battery curve ... 100%@12.7V -> 10%@11.31V, 0%@10.5V
Thank you
Clinton,