According to datasheet, SDA pin and SCL pin are I/O but SMBD and SMBC are I/OD. If SDA and SCL are I/O, can it still be connected on standard I2C bus? When it is connected with BQ79640, will it latch the data line because it is I/O pin but not open-drain pins?
Pin 3 SDA I/O Data transfer to and from the bq769x0 AFE. Requires a 10-k pullup to VCC
Pin 4 SCL I/O Communication clock to the bq769x0 AFE. Requires a 10-k pullup to VCC
Pin 11 SMBD I/OD SMBus data open-drain bidirectional pin used to transfer an address and data to and from the bq78350-R1 device
Pin 13 SMBC I/OD SMBus clock open-drain bidirectional pin used to clock the data transfer to and from the bq78350-R1 device