Hi Sir, Madam,
Do you have simple reference design for BQ34Z100-G1?
My customer currently is studying the reference design for BQ34Z100-G1 EVM and realized the size can't fit their small board size application.
Hope to hear from you soon. Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir, Madam,
Do you have simple reference design for BQ34Z100-G1?
My customer currently is studying the reference design for BQ34Z100-G1 EVM and realized the size can't fit their small board size application.
Hope to hear from you soon. Thanks.
Hi Bryan,
Thanks for the advice. My customer has further enquiry:
1) The LEDs for P1 and P2 are required for capacity indication. Can the FETs be removed and LEDs direct connected to the pin? Any issue?
2) Any way to trigger the LEDs blinking to indicate battery capacity? Is it possible to have 2 alternative control input to trigger the LEDs blinking, for example 1 is from battery pack and 1 is from the end device?
Below is Maxim DS2788 which my customer using previously, there is a pin called "PIO" for the function, for your reference.
Hope to hear from you soon. Thanks.
Hi Bryan,
My customer using a FET as a switch, when there is a pull high from device, it will turn on the FET then REG25 will give 2.5V to VEN pin and LED light will display to show battery capacity.
This FET is in parallel to the push button switch for the LED display.
Does the design need an extra protection component if switch and FET are in parallel.
For the current limiting, a limiting resistors and a blocking diode are added.
Hope to hear from you soon. Thanks.
Hi Bryan,
Thanks for your reply.
My customer followed below connection in the BQ34Z100-G1 datasheet for 1-cell Li-ion reference schematic.
Voltage of P+ is from 3V-4.2V (Battery voltage)
The switch to be used is the same as the original design using the DS2788 so it looks ok.
May I know what is the FET rating to be used in parallel to the switch?
Hope to hear from you soon. Thanks.