This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27742-G1: Not able to read the SOC and other required information of my battery(Lithium Ion Cylindrical Battery-1400mAh)

Part Number: BQ27742-G1
Other Parts Discussed in Thread: GPCCHEM, BQSTUDIO, EV2400

Hi ,

I am not getting battery information from fuel gauge. I have configured the fuel gauge from below parameter. is any correction required to configure the gauge?

is any extra work or parameter is need to get the battery information?

/*

//1st-class ID,2nd-offset,3rd-data,4th-length

{48, 12, 1400 ,2}, /* Design Capacity = 1400mAh */
{48, 14, 5180,2}, /* Design Energy = 3.7 * Design Capacity  */
{48, 00, 3700 ,2}, /* Design voltage = 1400mAh */

{34,00,4200,2}, /*charging voltage*/

{80, 64, 3600, 2}, /*terminate voltage  */

{2 , 5, 3600, 2}, /* UV Prot Threshold 3600 mV */
{2 , 8, 3700, 2}, /* UV Prot Recovery 3700 Mv */

{2 , 0, 4200, 2}, /* OV Prot Threshold 4200 mV */
{2 , 3, 4100, 2}, /* OV Prot Recovery 4100 Mv */

{36 , 0, 100, 2}, /* Taper current */
{36 , 4, 4200, 2} /* Taper voltage */

*/

Thanks,

Bhavna Harani

  • -you need to identify your chem id using our online tool gpcchem and then program on the device

    -then you need to perform a learning cycle following the app note attached before the gauge will be fully functional.

    8726.LearningCycleOverview_.pdf

    thanks

    Onyx

  • Hi Onyx,

    Thanks for Response.

    I am accessing Fuel gauge using Host controller I2c Interface. so, I am  Reading and writing of this gauge registers using commands.

    How I will get the chemistry ID for the " TENERGY Li-ion 18500 3.7v 1400mAh" battery.? can I config it from Host controller?

    Is it necessary to purchase the EVM board to configure  the fuel  gauge using Bqstudio or can use bqstudio without EVM board ? 

    As I have no much Idea about this  so  please give  more information regarding  this.

    Thanks.

    Bhavna 

  • Hi Bhavna,
    You cannot program the chem id using your host. You have to use bqstudio to program the chem id. You can use your board and the ev2300 or ev2400 and connect to a computer to be able to use bqstudio. See the evm user guide for instructions on the connections. I would recommend getting an evm to facilitate ease of configuration and golden file generation.
    thanks
    Onyx
  • Hi Onyx,

    Thank you so much for your response.

    We are going to place the order for the EVM board.

    Still I have question,In mass production like 5k quantity need to configure all gauges one by one?

    can you suggest  the steps for the mass production ?

    Thanks.

    Bhavna

  • hi Bhava,
    You will have to write code to parse the golden dffs file on the guage using your host aftter you are done configuring the gauge and performing your learning cycle.
    see attached app note

    www.ti.com/.../slua801

    thanks

    Onyx
  • soc1.log
    Wed Apr 25 18:59:29 IST 2018
    
    Device Name = bq27742G1
    Firmware Version = 1_03
    
    
    Sample,DateTime,ElapsedTime,Control,CtrlStatus,UnfilteredSOC,Temperature,Voltage,Flags,NomAvailCap,FullAvailCap,RemCap,FullChgCap,AvgCurrent,TimeToEmpty,FilteredFCC,SafetyStat,UnfilteredFCC,MaxCurrent,UnfilteredRM,FilteredRM,BTPSOC1Set,BTPSOC1Clear,IntTemp,CycleCnt,StateofCharge,StateofHealth,ChargeVoltage,ChargeCurrent,Passed Charge,DOD0,SelfDischargeCurrent,PackConfig,DoDatEOC,Qstart,Fast Qmax,Prot Stat,Int Stat,FET Test,Prot State,LogRowTime(ms),LogStatus
    1,2018-04-25 18:59:33,4.002,0x0103,0x600D,100,26.7,4165,0x001C,1012,1012,958,968,315,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-284,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,922,SUCCESS
    2,2018-04-25 18:59:37,8.001,0x0103,0x600D,100,26.7,4165,0x001C,1012,1012,958,968,314,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-284,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,917,SUCCESS
    3,2018-04-25 18:59:41,12.001,0x0103,0x600D,100,26.7,4165,0x001C,1012,1012,958,968,315,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-285,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,910,SUCCESS
    4,2018-04-25 18:59:45,16.001,0x0103,0x600D,100,26.7,4165,0x001C,1012,1012,958,968,314,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-285,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,919,SUCCESS
    5,2018-04-25 18:59:49,20.001,0x0103,0x600D,100,26.7,4165,0x001C,1012,1012,958,968,314,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-285,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,913,SUCCESS
    6,2018-04-25 18:59:53,24.002,0x0103,0x600D,100,26.7,4165,0x001C,1012,1012,958,968,313,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-286,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,922,SUCCESS
    7,2018-04-25 18:59:57,28.002,0x0103,0x600D,100,26.7,4165,0x001C,1012,1012,958,968,313,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-286,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,914,SUCCESS
    8,2018-04-25 19:00:01,32.002,0x0103,0x600D,100,26.7,4165,0x001C,1012,1012,958,968,313,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-286,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,924,SUCCESS
    9,2018-04-25 19:00:05,36.002,0x0103,0x600D,100,26.7,4165,0x001C,1012,1012,958,968,313,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-287,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,918,SUCCESS
    10,2018-04-25 19:00:09,40.003,0x0103,0x600D,100,26.7,4165,0x001C,1012,1012,958,968,313,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-287,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,910,SUCCESS
    11,2018-04-25 19:00:13,44.003,0x0103,0x600D,100,26.7,4166,0x001C,1012,1012,958,968,313,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-287,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,919,SUCCESS
    12,2018-04-25 19:00:17,48.003,0x0103,0x600D,100,26.7,4166,0x001C,1012,1012,958,968,313,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-288,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,913,SUCCESS
    13,2018-04-25 19:00:21,52.003,0x0103,0x600D,100,26.7,4166,0x001C,1012,1012,958,968,312,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-288,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,923,SUCCESS
    14,2018-04-25 19:00:25,56.003,0x0103,0x600D,100,26.7,4166,0x001C,1012,1012,958,968,312,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-288,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,916,SUCCESS
    15,2018-04-25 19:00:29,60.004,0x0103,0x600D,100,26.7,4166,0x001C,1012,1012,958,968,313,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-289,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,908,SUCCESS
    16,2018-04-25 19:00:33,64.004,0x0103,0x600D,100,26.7,4166,0x001C,1012,1012,958,968,312,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-289,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,918,SUCCESS
    17,2018-04-25 19:00:37,68.004,0x0103,0x600D,100,26.7,4166,0x001C,1012,1012,958,968,312,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-289,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,912,SUCCESS
    18,2018-04-25 19:00:41,72.004,0x0103,0x600D,100,26.7,4166,0x001C,1012,1012,958,968,311,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-290,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,920,SUCCESS
    19,2018-04-25 19:00:45,76.005,0x0103,0x600D,100,26.7,4166,0x001C,1012,1012,958,968,311,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-290,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,913,SUCCESS
    20,2018-04-25 19:00:49,80.005,0x0103,0x600D,100,26.7,4166,0x001C,1012,1012,958,968,310,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-290,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,923,SUCCESS
    21,2018-04-25 19:00:53,84.005,0x0103,0x600D,100,26.7,4167,0x001C,1012,1012,958,968,310,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-291,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,917,SUCCESS
    22,2018-04-25 19:00:57,88.005,0x0103,0x600D,100,26.7,4166,0x001C,1012,1012,958,968,310,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-291,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,909,SUCCESS
    23,2018-04-25 19:01:01,92.006,0x0103,0x600D,100,26.7,4167,0x001C,1012,1012,958,968,310,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-291,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,918,SUCCESS
    24,2018-04-25 19:01:05,96.006,0x0103,0x600D,100,26.7,4167,0x001C,1012,1012,958,968,310,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-292,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,912,SUCCESS
    25,2018-04-25 19:01:09,100.006,0x0103,0x600D,100,26.7,4167,0x001C,1012,1012,958,968,309,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-292,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,921,SUCCESS
    26,2018-04-25 19:01:13,104.006,0x0103,0x600D,100,26.7,4167,0x001C,1012,1012,958,968,309,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-292,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,914,SUCCESS
    27,2018-04-25 19:01:17,108.006,0x0103,0x600D,100,26.7,4167,0x001C,1012,1012,958,968,309,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-293,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,924,SUCCESS
    28,2018-04-25 19:01:21,112.007,0x0103,0x600D,100,26.7,4167,0x001C,1012,1012,958,968,308,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-293,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,917,SUCCESS
    29,2018-04-25 19:01:25,116.007,0x0103,0x600D,100,26.7,4167,0x001C,1012,1012,958,968,308,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-293,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,911,SUCCESS
    30,2018-04-25 19:01:29,120.007,0x0103,0x600D,100,26.7,4167,0x001C,1012,1012,958,968,308,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-294,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,919,SUCCESS
    31,2018-04-25 19:01:33,124.007,0x0103,0x600D,100,26.7,4167,0x001C,1012,1012,958,968,307,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-294,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,912,SUCCESS
    32,2018-04-25 19:01:37,128.008,0x0103,0x600D,100,26.7,4167,0x001C,1012,1012,958,968,307,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-294,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,922,SUCCESS
    33,2018-04-25 19:01:41,132.008,0x0103,0x600D,100,26.7,4168,0x001C,1012,1012,958,968,307,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-295,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,915,SUCCESS
    34,2018-04-25 19:01:45,136.008,0x0103,0x600D,100,26.7,4168,0x001C,1012,1012,958,968,306,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-295,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,923,SUCCESS
    35,2018-04-25 19:01:49,140.008,0x0103,0x600D,100,26.7,4168,0x001C,1012,1012,958,968,307,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-295,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,917,SUCCESS
    36,2018-04-25 19:01:53,144.009,0x0103,0x600D,100,26.7,4168,0x001C,1012,1012,958,968,306,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-296,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,911,SUCCESS
    37,2018-04-25 19:01:57,148.009,0x0103,0x600D,100,26.7,4168,0x001C,1012,1012,958,968,305,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-296,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,920,SUCCESS
    38,2018-04-25 19:02:01,152.009,0x0103,0x600D,100,26.7,4168,0x001C,1012,1012,958,968,305,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-296,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,913,SUCCESS
    39,2018-04-25 19:02:05,156.009,0x0103,0x600D,100,26.7,4168,0x001C,1012,1012,958,968,305,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-297,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,922,SUCCESS
    40,2018-04-25 19:02:09,160.009,0x0103,0x600D,100,26.7,4168,0x001C,1012,1012,958,968,306,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-297,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,916,SUCCESS
    41,2018-04-25 19:02:13,164.010,0x0103,0x600D,100,26.7,4169,0x001C,1012,1012,958,968,305,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-297,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,909,SUCCESS
    42,2018-04-25 19:02:17,168.010,0x0103,0x600D,100,26.7,4168,0x001C,1012,1012,958,968,305,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-298,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,917,SUCCESS
    43,2018-04-25 19:02:21,172.010,0x0103,0x600D,100,26.7,4168,0x001C,1012,1012,958,968,304,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-298,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,912,SUCCESS
    44,2018-04-25 19:02:25,176.010,0x0103,0x600D,100,26.7,4169,0x001C,1012,1012,958,968,305,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-298,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,921,SUCCESS
    45,2018-04-25 19:02:29,180.011,0x0103,0x600D,100,26.7,4168,0x001C,1012,1012,958,968,304,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-299,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,914,SUCCESS
    46,2018-04-25 19:02:33,184.011,0x0103,0x600D,100,26.7,4169,0x001C,1012,1012,958,968,303,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-299,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,922,SUCCESS
    47,2018-04-25 19:02:37,188.011,0x0103,0x600D,100,26.7,4169,0x001C,1012,1012,958,968,303,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-299,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,917,SUCCESS
    48,2018-04-25 19:02:41,192.011,0x0103,0x600D,100,26.7,4169,0x001C,1012,1012,958,968,303,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-300,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,910,SUCCESS
    49,2018-04-25 19:02:45,196.012,0x0103,0x600D,100,26.7,4169,0x001C,1012,1012,958,968,303,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-300,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,919,SUCCESS
    50,2018-04-25 19:02:49,200.012,0x0103,0x600D,100,26.7,4169,0x001C,1012,1012,958,968,302,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-300,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,911,SUCCESS
    51,2018-04-25 19:02:53,204.012,0x0103,0x600D,100,26.7,4169,0x001C,1012,1012,958,968,302,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-301,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,921,SUCCESS
    52,2018-04-25 19:02:57,208.012,0x0103,0x600D,100,26.7,4169,0x001C,1012,1012,958,968,303,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-301,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,915,SUCCESS
    53,2018-04-25 19:03:01,212.012,0x0103,0x600D,100,26.7,4170,0x001C,1012,1012,958,968,302,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-301,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,923,SUCCESS
    54,2018-04-25 19:03:05,216.013,0x0103,0x600D,100,26.7,4170,0x001C,1012,1012,958,968,302,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-302,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,916,SUCCESS
    55,2018-04-25 19:03:09,220.013,0x0103,0x600D,100,26.7,4169,0x001C,1012,1012,958,968,302,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-302,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,910,SUCCESS
    56,2018-04-25 19:03:13,224.013,0x0103,0x600D,100,26.7,4170,0x001C,1012,1012,958,968,302,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-302,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,919,SUCCESS
    57,2018-04-25 19:03:17,228.013,0x0103,0x600D,100,26.7,4170,0x001C,1012,1012,958,968,302,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-303,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,912,SUCCESS
    58,2018-04-25 19:03:21,232.014,0x0103,0x600D,100,26.7,4170,0x001C,1012,1012,958,968,301,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-303,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,921,SUCCESS
    59,2018-04-25 19:03:25,236.014,0x0103,0x600D,100,26.7,4171,0x001C,1012,1012,958,968,300,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-303,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,915,SUCCESS
    60,2018-04-25 19:03:29,240.014,0x0103,0x600D,100,26.7,4170,0x001C,1012,1012,958,968,301,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-304,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,924,SUCCESS
    61,2018-04-25 19:03:33,244.014,0x0103,0x600D,100,26.7,4171,0x001C,1012,1012,958,968,299,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-304,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,917,SUCCESS
    62,2018-04-25 19:03:37,248.014,0x0103,0x600D,100,26.7,4171,0x001C,1012,1012,958,968,299,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-304,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,911,SUCCESS
    63,2018-04-25 19:03:41,252.015,0x0103,0x600D,100,26.7,4172,0x001C,1012,1012,958,968,300,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-305,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,920,SUCCESS
    64,2018-04-25 19:03:45,256.015,0x0103,0x600D,100,26.7,4171,0x001C,1012,1012,958,968,299,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-305,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,913,SUCCESS
    65,2018-04-25 19:03:49,260.015,0x0103,0x600D,100,26.7,4171,0x001C,1012,1012,958,968,298,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-305,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,921,SUCCESS
    66,2018-04-25 19:03:53,264.015,0x0103,0x600D,100,26.7,4172,0x001C,1012,1012,958,968,299,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-306,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,915,SUCCESS
    67,2018-04-25 19:03:57,268.016,0x0103,0x600D,100,26.7,4171,0x001C,1012,1012,958,968,298,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-306,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,909,SUCCESS
    68,2018-04-25 19:04:01,272.016,0x0103,0x600D,100,26.7,4172,0x001C,1012,1012,958,968,298,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-306,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,918,SUCCESS
    69,2018-04-25 19:04:05,276.016,0x0103,0x600D,100,26.7,4172,0x001C,1012,1012,958,968,298,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-307,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,911,SUCCESS
    70,2018-04-25 19:04:09,280.016,0x0103,0x600D,100,26.7,4172,0x001C,1012,1012,958,968,298,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-307,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,920,SUCCESS
    71,2018-04-25 19:04:13,284.017,0x0103,0x600D,100,26.7,4172,0x001C,1012,1012,958,968,297,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-307,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,914,SUCCESS
    72,2018-04-25 19:04:17,288.017,0x0103,0x600D,100,26.7,4172,0x001C,1012,1012,958,968,298,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-308,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,923,SUCCESS
    73,2018-04-25 19:04:21,292.017,0x0103,0x600D,100,26.7,4172,0x001C,1012,1012,958,968,296,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-308,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,915,SUCCESS
    74,2018-04-25 19:04:25,296.017,0x0103,0x600D,100,26.7,4172,0x001C,1012,1012,958,968,297,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-308,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,910,SUCCESS
    75,2018-04-25 19:04:29,300.017,0x0103,0x600D,100,26.7,4173,0x001C,1012,1012,958,968,296,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-309,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,920,SUCCESS
    76,2018-04-25 19:04:33,304.018,0x0103,0x600D,100,26.7,4173,0x001C,1012,1012,958,968,296,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-309,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,912,SUCCESS
    77,2018-04-25 19:04:37,308.018,0x0103,0x600D,100,26.7,4173,0x001C,1012,1012,958,968,297,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-309,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,920,SUCCESS
    78,2018-04-25 19:04:41,312.018,0x0103,0x600D,100,26.7,4173,0x001C,1012,1012,958,968,295,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-309,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,915,SUCCESS
    79,2018-04-25 19:04:45,316.018,0x0103,0x600D,100,26.7,4173,0x001C,1012,1012,958,968,295,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-310,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,924,SUCCESS
    80,2018-04-25 19:04:49,320.019,0x0103,0x600D,100,26.7,4173,0x001C,1012,1012,958,968,295,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-310,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,916,SUCCESS
    81,2018-04-25 19:04:53,324.019,0x0103,0x600D,100,26.7,4173,0x001C,1012,1012,958,968,295,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-310,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,909,SUCCESS
    82,2018-04-25 19:04:57,328.019,0x0103,0x600D,100,26.7,4173,0x001C,1012,1012,958,968,295,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-311,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,919,SUCCESS
    83,2018-04-25 19:05:01,332.019,0x0103,0x600D,100,26.7,4173,0x001C,1012,1012,958,968,294,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-311,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,913,SUCCESS
    84,2018-04-25 19:05:05,336.020,0x0103,0x600D,100,26.7,4173,0x001C,1012,1012,958,968,293,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-311,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,921,SUCCESS
    85,2018-04-25 19:05:09,340.020,0x0103,0x600D,100,26.7,4174,0x001C,1012,1012,958,968,294,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-312,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,914,SUCCESS
    86,2018-04-25 19:05:13,344.020,0x0103,0x600D,100,26.7,4174,0x001C,1012,1012,958,968,294,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-312,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,924,SUCCESS
    87,2018-04-25 19:05:17,348.020,0x0103,0x600D,100,26.7,4174,0x001C,1012,1012,958,968,294,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-312,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,918,SUCCESS
    88,2018-04-25 19:05:21,352.020,0x0103,0x600D,100,26.7,4174,0x001C,1012,1012,958,968,294,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-313,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,910,SUCCESS
    89,2018-04-25 19:05:25,356.021,0x0103,0x600D,100,26.7,4174,0x001C,1012,1012,958,968,293,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-313,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,919,SUCCESS
    90,2018-04-25 19:05:29,360.021,0x0103,0x600D,100,26.7,4174,0x001C,1012,1012,958,968,293,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-313,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,913,SUCCESS
    91,2018-04-25 19:05:33,364.021,0x0103,0x600D,100,26.7,4174,0x001C,1012,1012,958,968,293,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-314,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,922,SUCCESS
    92,2018-04-25 19:05:37,368.021,0x0103,0x600D,100,26.7,4174,0x001C,1012,1012,958,968,292,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-314,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,915,SUCCESS
    93,2018-04-25 19:05:41,372.022,0x0103,0x600D,100,26.7,4175,0x001C,1012,1012,958,968,292,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-314,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,924,SUCCESS
    94,2018-04-25 19:05:45,376.022,0x0103,0x600D,100,26.7,4175,0x001C,1012,1012,958,968,292,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-315,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,918,SUCCESS
    95,2018-04-25 19:05:49,380.022,0x0103,0x600D,100,26.7,4174,0x001C,1012,1012,958,968,291,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-315,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,912,SUCCESS
    96,2018-04-25 19:05:53,384.022,0x0103,0x600D,100,26.7,4175,0x001C,1012,1012,958,968,292,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-315,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,920,SUCCESS
    97,2018-04-25 19:05:57,388.022,0x0103,0x600D,100,26.7,4175,0x001C,1012,1012,958,968,291,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-316,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,914,SUCCESS
    98,2018-04-25 19:06:01,392.023,0x0103,0x600D,100,26.7,4175,0x001C,1012,1012,958,968,290,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-316,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,923,SUCCESS
    99,2018-04-25 19:06:05,396.023,0x0103,0x600D,100,26.7,4175,0x001C,1012,1012,958,968,290,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-316,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,916,SUCCESS
    100,2018-04-25 19:06:09,400.023,0x0103,0x600D,100,26.7,4175,0x001C,1012,1012,958,968,291,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-317,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,909,SUCCESS
    101,2018-04-25 19:06:13,404.023,0x0103,0x600D,100,26.7,4175,0x001C,1012,1012,958,968,291,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-317,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,918,SUCCESS
    102,2018-04-25 19:06:17,408.024,0x0103,0x600D,100,26.7,4176,0x001C,1012,1012,958,968,290,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-317,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,912,SUCCESS
    103,2018-04-25 19:06:21,412.024,0x0103,0x600D,100,26.7,4175,0x001C,1012,1012,958,968,290,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-317,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,921,SUCCESS
    104,2018-04-25 19:06:25,416.024,0x0103,0x600D,100,26.7,4175,0x001C,1012,1012,958,968,290,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-318,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,914,SUCCESS
    105,2018-04-25 19:06:29,420.024,0x0103,0x600D,100,26.7,4176,0x001C,1012,1012,958,968,289,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-318,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,923,SUCCESS
    106,2018-04-25 19:06:33,424.025,0x0103,0x600D,100,26.7,4176,0x001C,1012,1012,958,968,289,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-318,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,917,SUCCESS
    107,2018-04-25 19:06:37,428.025,0x0103,0x600D,100,26.7,4176,0x001C,1012,1012,958,968,288,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-319,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,910,SUCCESS
    108,2018-04-25 19:06:41,432.025,0x0103,0x600D,100,26.7,4176,0x001C,1012,1012,958,968,289,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-319,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,918,SUCCESS
    109,2018-04-25 19:06:45,436.025,0x0103,0x600D,100,26.7,4176,0x001C,1012,1012,958,968,288,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-319,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,912,SUCCESS
    110,2018-04-25 19:06:49,440.025,0x0103,0x600D,100,26.7,4175,0x001C,1012,1012,958,968,283,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-320,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,923,SUCCESS
    111,2018-04-25 19:06:53,444.026,0x0103,0x600D,100,26.7,4176,0x001C,1012,1012,958,968,284,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-320,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,915,SUCCESS
    112,2018-04-25 19:06:57,448.026,0x0103,0x600D,100,26.7,4175,0x001C,1012,1012,958,968,284,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-320,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,923,SUCCESS
    113,2018-04-25 19:07:01,452.026,0x0103,0x600D,100,26.7,4176,0x001C,1012,1012,958,968,283,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-321,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,917,SUCCESS
    114,2018-04-25 19:07:05,456.026,0x0103,0x600D,100,26.7,4176,0x001C,1012,1012,958,968,284,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-321,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,911,SUCCESS
    115,2018-04-25 19:07:09,460.027,0x0103,0x600D,100,26.7,4177,0x001C,1012,1012,958,968,283,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-321,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,920,SUCCESS
    116,2018-04-25 19:07:13,464.027,0x0103,0x600D,100,26.7,4176,0x001C,1012,1012,958,968,283,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-322,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,912,SUCCESS
    117,2018-04-25 19:07:17,468.027,0x0103,0x600D,100,26.7,4176,0x001C,1012,1012,958,968,283,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-322,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,922,SUCCESS
    118,2018-04-25 19:07:21,472.027,0x0103,0x600D,100,26.7,4177,0x001C,1012,1012,958,968,283,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-322,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,916,SUCCESS
    119,2018-04-25 19:07:25,476.028,0x0103,0x600D,100,26.7,4177,0x001C,1012,1012,958,968,282,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-322,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,925,SUCCESS
    120,2018-04-25 19:07:29,480.028,0x0103,0x600D,100,26.7,4177,0x001C,1012,1012,958,968,282,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-323,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,917,SUCCESS
    121,2018-04-25 19:07:33,484.028,0x0103,0x600D,100,26.7,4177,0x001C,1012,1012,958,968,283,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-323,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,911,SUCCESS
    122,2018-04-25 19:07:37,488.028,0x0103,0x600D,100,26.7,4177,0x001C,1012,1012,958,968,282,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-323,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,920,SUCCESS
    123,2018-04-25 19:07:41,492.028,0x0103,0x600D,100,26.8,4177,0x001C,1012,1012,958,968,281,65535,968,0x0,968,6165,968,968,150,175,24.2,11,99,71,4350,1120,-324,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,913,SUCCESS
    124,2018-04-25 19:07:45,496.029,0x0103,0x600D,100,26.8,4177,0x001C,1012,1012,958,968,281,65535,968,0x0,968,6165,968,968,150,175,24.2,11,99,71,4350,1120,-324,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,922,SUCCESS
    125,2018-04-25 19:07:49,500.029,0x0103,0x600D,100,26.8,4177,0x001C,1012,1012,958,968,281,65535,968,0x0,968,6165,968,968,150,175,24.2,11,99,71,4350,1120,-324,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,916,SUCCESS
    126,2018-04-25 19:07:53,504.029,0x0103,0x600D,100,26.8,4178,0x001C,1012,1012,958,968,281,65535,968,0x0,968,6165,968,968,150,175,24.2,11,99,71,4350,1120,-325,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,910,SUCCESS
    127,2018-04-25 19:07:57,508.029,0x0103,0x600D,100,26.8,4177,0x001C,1012,1012,958,968,281,65535,968,0x0,968,6165,968,968,150,175,24.2,11,99,71,4350,1120,-325,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,918,SUCCESS
    128,2018-04-25 19:08:01,512.030,0x0103,0x600D,100,26.8,4178,0x001C,1012,1012,958,968,281,65535,968,0x0,968,6165,968,968,150,175,24.2,11,99,71,4350,1120,-325,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,911,SUCCESS
    129,2018-04-25 19:08:05,516.030,0x0103,0x600D,100,26.8,4178,0x001C,1012,1012,958,968,281,65535,968,0x0,968,6165,968,968,150,175,24.2,11,99,71,4350,1120,-326,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,921,SUCCESS
    130,2018-04-25 19:08:09,520.030,0x0103,0x600D,100,26.8,4178,0x001C,1012,1012,958,968,281,65535,968,0x0,968,6165,968,968,150,175,24.2,11,99,71,4350,1120,-326,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,914,SUCCESS
    131,2018-04-25 19:08:13,524.030,0x0103,0x600D,100,26.8,4178,0x001C,1012,1012,958,968,281,65535,968,0x0,968,6165,968,968,150,175,24.2,11,99,71,4350,1120,-326,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,923,SUCCESS
    132,2018-04-25 19:08:17,528.030,0x0103,0x600D,100,26.8,4178,0x001C,1012,1012,958,968,281,65535,968,0x0,968,6165,968,968,150,175,24.2,11,99,71,4350,1120,-326,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,917,SUCCESS
    133,2018-04-25 19:08:21,532.031,0x0103,0x600D,100,26.7,4178,0x001C,1012,1012,958,968,281,65535,968,0x0,968,6165,968,968,150,175,24.2,11,99,71,4350,1120,-327,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,910,SUCCESS
    134,2018-04-25 19:08:25,536.031,0x0103,0x600D,100,26.8,4178,0x001C,1012,1012,958,968,281,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-327,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,919,SUCCESS
    135,2018-04-25 19:08:29,540.031,0x0103,0x600D,100,26.7,4179,0x001C,1012,1012,958,968,280,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-327,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,912,SUCCESS
    136,2018-04-25 19:08:33,544.031,0x0103,0x600D,100,26.7,4179,0x001C,1012,1012,958,968,280,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-328,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,921,SUCCESS
    137,2018-04-25 19:08:37,548.032,0x0103,0x600D,100,26.7,4178,0x001C,1012,1012,958,968,280,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-328,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,915,SUCCESS
    138,2018-04-25 19:08:41,552.032,0x0103,0x600D,100,26.7,4179,0x001C,1012,1012,958,968,281,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-328,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,924,SUCCESS
    139,2018-04-25 19:08:45,556.032,0x0103,0x600D,100,26.7,4179,0x001C,1012,1012,958,968,280,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-329,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,916,SUCCESS
    140,2018-04-25 19:08:49,560.032,0x0103,0x600D,100,26.7,4180,0x001C,1012,1012,958,968,280,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-329,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,910,SUCCESS
    141,2018-04-25 19:08:53,564.033,0x0103,0x600D,100,26.7,4180,0x001C,1012,1012,958,968,280,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-329,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,920,SUCCESS
    142,2018-04-25 19:08:57,568.033,0x0103,0x600D,100,26.7,4179,0x001C,1012,1012,958,968,279,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-330,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,913,SUCCESS
    143,2018-04-25 19:09:01,572.033,0x0103,0x600D,100,26.7,4180,0x001C,1012,1012,958,968,279,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-330,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,921,SUCCESS
    144,2018-04-25 19:09:05,576.033,0x0103,0x600D,100,26.7,4180,0x001C,1012,1012,958,968,279,65535,968,0x0,968,6154,968,968,150,175,24.1,11,99,71,4350,1120,-330,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,916,SUCCESS
    145,2018-04-25 19:09:09,580.033,0x0103,0x600D,100,26.7,4180,0x001C,1012,1012,958,968,279,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-330,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,926,SUCCESS
    146,2018-04-25 19:09:13,584.034,0x0103,0x600D,100,26.7,4180,0x001C,1012,1012,958,968,279,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-331,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,918,SUCCESS
    147,2018-04-25 19:09:17,588.034,0x0103,0x600D,100,26.7,4180,0x001C,1012,1012,958,968,279,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-331,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,910,SUCCESS
    148,2018-04-25 19:09:21,592.034,0x0103,0x600D,100,26.7,4181,0x001C,1012,1012,958,968,278,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-331,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,920,SUCCESS
    149,2018-04-25 19:09:25,596.034,0x0103,0x600D,100,26.7,4181,0x001C,1012,1012,958,968,278,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-332,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,914,SUCCESS
    150,2018-04-25 19:09:29,600.035,0x0103,0x600D,100,26.7,4180,0x001C,1012,1012,958,968,278,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-332,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,923,SUCCESS
    151,2018-04-25 19:09:33,604.035,0x0103,0x600D,100,26.7,4181,0x001C,1012,1012,958,968,277,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-332,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,915,SUCCESS
    152,2018-04-25 19:09:37,608.035,0x0103,0x600D,100,26.7,4180,0x001C,1012,1012,958,968,277,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-332,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,909,SUCCESS
    153,2018-04-25 19:09:41,612.035,0x0103,0x600D,100,26.7,4181,0x001C,1012,1012,958,968,277,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-333,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,919,SUCCESS
    154,2018-04-25 19:09:45,616.036,0x0103,0x600D,100,26.7,4181,0x001C,1012,1012,958,968,276,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-333,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,912,SUCCESS
    155,2018-04-25 19:09:49,620.036,0x0103,0x600D,100,26.8,4181,0x001C,1012,1012,958,968,276,65535,968,0x0,968,6165,968,968,150,175,24.2,11,99,71,4350,1120,-333,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,920,SUCCESS
    156,2018-04-25 19:09:53,624.036,0x0103,0x600D,100,26.8,4181,0x001C,1012,1012,958,968,276,65535,968,0x0,968,6165,968,968,150,175,24.2,11,99,71,4350,1120,-334,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,914,SUCCESS
    157,2018-04-25 19:09:57,628.036,0x0103,0x600D,100,26.7,4181,0x001C,1012,1012,958,968,276,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-334,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,923,SUCCESS
    158,2018-04-25 19:10:01,632.036,0x0103,0x600D,100,26.7,4181,0x001C,1012,1012,958,968,276,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-334,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,916,SUCCESS
    159,2018-04-25 19:10:05,636.037,0x0103,0x600D,100,26.8,4181,0x001C,1012,1012,958,968,275,65535,968,0x0,968,6165,968,968,150,175,24.2,11,99,71,4350,1120,-335,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,909,SUCCESS
    160,2018-04-25 19:10:09,640.037,0x0103,0x600D,100,26.7,4181,0x001C,1012,1012,958,968,274,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-335,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,919,SUCCESS
    161,2018-04-25 19:10:13,644.037,0x0103,0x600D,100,26.7,4182,0x001C,1012,1012,958,968,274,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-335,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,913,SUCCESS
    162,2018-04-25 19:10:17,648.037,0x0103,0x600D,100,26.7,4182,0x001C,1012,1012,958,968,274,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-335,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,921,SUCCESS
    163,2018-04-25 19:10:21,652.038,0x0103,0x600D,100,26.7,4182,0x001C,1012,1012,958,968,274,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-336,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,914,SUCCESS
    164,2018-04-25 19:10:25,656.038,0x0103,0x600D,100,26.7,4182,0x001C,1012,1012,958,968,274,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-336,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,924,SUCCESS
    165,2018-04-25 19:10:29,660.038,0x0103,0x600D,100,26.7,4182,0x001C,1012,1012,958,968,274,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-336,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,917,SUCCESS
    166,2018-04-25 19:10:33,664.038,0x0103,0x600D,100,26.7,4182,0x001C,1012,1012,958,968,273,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-337,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,911,SUCCESS
    167,2018-04-25 19:10:37,668.038,0x0103,0x600D,100,26.7,4182,0x001C,1012,1012,958,968,273,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-337,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,920,SUCCESS
    168,2018-04-25 19:10:41,672.039,0x0103,0x600D,100,26.7,4183,0x001C,1012,1012,958,968,273,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-337,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,913,SUCCESS
    169,2018-04-25 19:10:45,676.039,0x0103,0x600D,100,26.7,4183,0x001C,1012,1012,958,968,273,65535,968,0x0,968,6154,968,968,150,175,24.2,11,99,71,4350,1120,-338,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,922,SUCCESS
    170,2018-04-25 19:10:49,680.039,0x0103,0x600D,100,26.8,4183,0x001C,1012,1012,958,968,272,65535,968,0x0,968,6165,968,968,150,175,24.2,11,99,71,4350,1120,-338,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,915,SUCCESS
    171,2018-04-25 19:10:53,684.039,0x0103,0x600D,100,26.8,4183,0x001C,1012,1012,958,968,272,65535,968,0x0,968,6165,968,968,150,175,24.2,11,99,71,4350,1120,-338,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,924,SUCCESS
    172,2018-04-25 19:10:57,688.040,0x0103,0x600D,100,26.8,4183,0x001C,1012,1012,958,968,272,65535,968,0x0,968,6165,968,968,150,175,24.2,11,99,71,4350,1120,-338,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,918,SUCCESS
    173,2018-04-25 19:11:01,692.040,0x0103,0x600D,100,26.8,4183,0x001C,1012,1012,958,968,271,65535,968,0x0,968,6165,968,968,150,175,24.2,11,99,71,4350,1120,-339,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,911,SUCCESS
    174,2018-04-25 19:11:05,696.040,0x0103,0x600D,100,26.8,4183,0x001C,1012,1012,958,968,272,65535,968,0x0,968,6165,968,968,150,175,24.2,11,99,71,4350,1120,-339,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,919,SUCCESS
    175,2018-04-25 19:11:09,700.040,0x0103,0x600D,100,26.8,4183,0x001C,1012,1012,958,968,271,65535,968,0x0,968,6165,968,968,150,175,24.2,11,99,71,4350,1120,-339,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,913,SUCCESS
    176,2018-04-25 19:11:13,704.041,0x0103,0x600D,100,26.8,4184,0x001C,1012,1012,958,968,271,65535,968,0x0,968,6165,968,968,150,175,24.2,11,99,71,4350,1120,-340,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,923,SUCCESS
    177,2018-04-25 19:11:17,708.041,0x0103,0x600D,100,26.8,4184,0x001C,1012,1012,958,968,271,65535,968,0x0,968,6165,968,968,150,175,24.2,11,99,71,4350,1120,-340,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,916,SUCCESS
    178,2018-04-25 19:11:21,712.041,0x0103,0x600D,100,26.8,4184,0x001C,1012,1012,958,968,269,65535,968,0x0,968,6165,968,968,150,175,24.2,11,99,71,4350,1120,-340,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,909,SUCCESS
    179,2018-04-25 19:11:25,716.041,0x0103,0x600D,100,26.8,4184,0x001C,1012,1012,958,968,269,65535,968,0x0,968,6165,968,968,150,175,24.2,11,99,71,4350,1120,-341,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,918,SUCCESS
    180,2018-04-25 19:11:29,720.041,0x0103,0x600D,100,26.8,4184,0x001C,1012,1012,958,968,269,65535,968,0x0,968,6165,968,968,150,175,24.3,11,99,71,4350,1120,-341,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,913,SUCCESS
    181,2018-04-25 19:11:33,724.042,0x0103,0x600D,100,26.8,4186,0x001C,1012,1012,958,968,268,65535,968,0x0,968,6165,968,968,150,175,24.2,11,99,71,4350,1120,-341,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,921,SUCCESS
    182,2018-04-25 19:11:37,728.042,0x0103,0x600D,100,26.8,4185,0x001C,1012,1012,958,968,268,65535,968,0x0,968,6165,968,968,150,175,24.2,11,99,71,4350,1120,-341,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,913,SUCCESS
    183,2018-04-25 19:11:41,732.042,0x0103,0x600D,100,26.8,4187,0x001C,1012,1012,958,968,267,65535,968,0x0,968,6165,968,968,150,175,24.3,11,99,71,4350,1120,-342,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,923,SUCCESS
    184,2018-04-25 19:11:45,736.042,0x0103,0x600D,100,26.8,4186,0x001C,1012,1012,958,968,267,65535,968,0x0,968,6165,968,968,150,175,24.3,11,99,71,4350,1120,-342,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,917,SUCCESS
    185,2018-04-25 19:11:49,740.043,0x0103,0x600D,100,26.8,4186,0x001C,1012,1012,958,968,267,65535,968,0x0,968,6165,968,968,150,175,24.3,11,99,71,4350,1120,-342,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,910,SUCCESS
    186,2018-04-25 19:11:53,744.043,0x0103,0x600D,100,26.8,4186,0x001C,1012,1012,958,968,266,65535,968,0x0,968,6165,968,968,150,175,24.3,11,99,71,4350,1120,-343,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,918,SUCCESS
    187,2018-04-25 19:11:57,748.043,0x0103,0x600D,100,26.8,4193,0x001C,1012,1012,958,968,259,65535,968,0x0,968,6165,968,968,150,175,24.3,11,99,71,4350,1120,-343,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,912,SUCCESS
    188,2018-04-25 19:12:01,752.043,0x0103,0x600D,100,26.8,4192,0x001C,1012,1012,958,968,260,65535,968,0x0,968,6165,968,968,150,175,24.2,11,99,71,4350,1120,-343,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,921,SUCCESS
    189,2018-04-25 19:12:05,756.044,0x0103,0x600D,100,26.8,4191,0x001C,1012,1012,958,968,260,65535,968,0x0,968,6165,968,968,150,175,24.2,11,99,71,4350,1120,-343,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,915,SUCCESS
    190,2018-04-25 19:12:09,760.044,0x0103,0x600D,100,26.8,4191,0x001C,1012,1012,958,968,260,65535,968,0x0,968,6165,968,968,150,175,24.2,11,99,71,4350,1120,-344,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,923,SUCCESS
    191,2018-04-25 19:12:13,764.044,0x0103,0x600D,100,26.8,4191,0x001C,1012,1012,958,968,260,65535,968,0x0,968,6165,968,968,150,175,24.3,11,99,71,4350,1120,-344,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,917,SUCCESS
    192,2018-04-25 19:12:17,768.044,0x0103,0x600D,100,26.8,4191,0x001C,1012,1012,958,968,260,65535,968,0x0,968,6165,968,968,150,175,24.2,11,99,71,4350,1120,-344,3008,0,0x097F,16,256,0,0x00,0x2200,0x0000,0x02,911,SUCCESS
    
    Hi Onyx,

    I am repeating my set up on which i am working.

    I am using TENERGY Li-ion battery. whose nominal voltage is 3.7v and capacity is 1400mAh.

    This battery's chemistry ID is not in TI's database.

    I found that,using GPC cycle i can get appropriate chemistry ID. For that i have purchased EVM2400 board.

    I have installed bqstudio version 1.3.54.1,in that i am not getting GPC cycle option. is there any updated version for bqstudio in that i get gpc cycle to get chemistry id?

    Below I have mention the test scenario ,and issue that i have faced

    - For testing purpose I have used 0x1305 chemistry ID. SOC of battery is not showing correctly.

    -When I am charging the battery ,SOC will increase ,but stop on 99%. i have attached log file. 

    -When I  am going to discharge the battery SOC will stay same.but it should decrease.


    please ,give me some hint on this. I have also followed documents  and video regarding this.

    will wait to hear from you.

  • Bhavna,

    You need to perform a learning cycle before the gauge can report SOC correctly.

    Attached is app note directing you on how to perform a successful learning cycle.

    8255.LearningCycleOverview_.pdf

    if your bqstudio does not have the gpcpackager, that is not a deal breaker. you can just follow the instructions in the manual for uploading your files to the tool. why do u need the packager? i thought you mentioned you had already identified a chem id match using the gpctool?

    thanks

    Onyx