Tool/software: TI C/C++ Compiler
hi all
Actually we’re facing an issue with pcm 9055 using bq 27541 G1 ,the battery management software showed a compatibility error between bq27541 G1 and bq27541 v200 ,then we used the bq evaluation software and we had a rondom temperature values between 76°C and -900°C ,SOC between 76% and 0% !! which is illogical .
We wonder to know if you have already used such kind of bq and dealt with BqEasy before, is there any suggestions to solve this problem?
and what s rom mode, how can i jump to it?