Other Parts Discussed in Thread: BQ34Z100
Hi,
I am using a BQ34z100-g1 with an 8s2p LiFePO4 batteries. I have one doubt about the Cell Termination Voltage.
¿What are the condictions that mus be met in the BQ for the SoC to go to 0%?
I have done two tests:
- Discharge the battery from 100% to this voltage (Cell Termination Voltage x 8 (number of cells)). Then the SoC falls to 0% (regardless of the SoC it had before reach this point)
- With battery at a high SoC(for example 70%) quit the battery (but not quit the BQ34z100-g1 power supply). Then the BQ shows voltage of 0mV but the SoC remains at 70%.
Is there any current consideration in addition to the Cell Voltage Termination that must be met for the SoC to go to 0%?
Best regards,