This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27531-G1: Restart new learning cycle (Update Status 0 = 0x02 blocked)

Part Number: BQ27531-G1
Other Parts Discussed in Thread: BQ27531EVM, , BQSTUDIO

Hello, 

I am using bq27531EVM and my new type of battery. I have followed the process mentioned in the documentation in order to adapt the gauge system for this type of battery. The seguence is as follows:

  1. Get Chemical ID:
    1. Perform a relax-charge-relax-discharge and then send the log (.zip) to web tool of TI.
    2. Program the ID reported in bq27531
  2. Perform a learning cycle:
    1. I have followed the procedure mentioned in different documents and after severals tries it seems to be working properly (Update status = 0x02, SoC evolution is working as expected)

However, when I try to repeat the learning process with another battery in order to compare the results I am not able to restart the procedure. The sequence I use is:

Initial conditions:

QEN = 1, Update Status = 0x02

Start procedure:

Send IT_ENABLE command

Send RESET command

At this point Update Status should be 0x00, but it is equal to 0x02. I think this is the problem. It seems as if the learning process has not finished properly and no new learning cycles can be initiated.

Could you help me?

Thanks,

Eduardo