Other Parts Discussed in Thread: GPCRA0
Hello;
My cell is Kokam SLPB080085270 (6S1P). Battery features;
- Max Voltage = 4.2V
- Min Voltage = 2.7V
- Capacity = 27000 mAh
The learning Cycle is completed. But there are problems in the last product. After taking the golden image, IT_Enable is being done.
Then the BMS is starting to be used. The SoC is resetting when the battery is about 17.5-18V. The log that is received about the subject is below. What is the problem in the last prouct? I think the problem is that the average current is not updated quickly during sudden current changes.