Welcome to the Battery Management Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".
Q: bq2000T application
Q1) Customer will use 8s NiMH cells, with a max cell voltage of 2V and a charge rate of C/4. What is min input voltage to support this? I am guessing its 16V plus a couple of volts overhead to allow for voltage drops. Is this enough or is there a more exact calculation?
A1) Yes, 16V is a good voltage (would not go below 15V minimum). It is normal for a range of charge current since the current can vary depending on the input voltage, output voltage and component tolerances. I would suggest a charge between C/3 and C/2 because one gets a more reliable termination at C/3 and above and since the current can vary 20 to 30%.