BQ2031 EVM...which one?

Q: BQ2031 EVM...which one?

There are two development systems for the BQ2031 listed in the product folder:

DV2031S1 Fast Charge Development System User's Guide

Which is the right one to use?


A: Re: BQ2031 EVM...which one?

I typically have used the S1, but I believe all that is different for the S2 is the use of a P-CH FET instead of a PNP.