bq24075 with no battery

Q: bq24075 with no battery by 1038028

Can user use this with the battery disconnected, but USB power connected?

Will it just pass USB powe straight though to power his system, no problem?

Q: Re: bq24075 with no battery by 1140793

Yes. User can use the OUT pin to power the system when a USB power is connected and the battery is disconnected. The Vo(reg) of bq24075 is 5.5V.

If the system load current is not higher than input current limit, bq24075 can pass USB power to the system. No problem.