Welcome to the Battery Management Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".
Q: BQ24103A_/CE pin impedance by 1300154
Hi,
A customer is using our bq24103A for their next TV set application, but now they have some trouble with it.
They did an ESD test and found that charge is terminated due to noise on CE pin.
They've added a 1uF bypass capacitor on CE pin and the problem seems to be solved.
Anyway, their question is
How much is impedance on the /CE pin of bq24103A??
From block diagram in the datasheet, signal from CE is directly inserted to a control logic circuit, and I think it's a comparator with megaohms impedance on its input.
Could someone tell me the approximate value of /CE pin impedance in bq24103A??
I'll need to answer this ASAP so please if somebody knows the answer could you please share.
Thank you in advance.
Q: Re: BQ24103A_/CE pin impedance by 8433
The datasheet gives V(IH) as 1.3V-VCC with I(IH)=20uA. So, a good estimate for the impedance minimum would be VCC(max)=16V/20uA = 800kohm.