Welcome to the Battery Management Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".
Q: bq27510-G1 Converting hex to floating point number by 1455674
Hi Everyone.
I am writing an application which can read the GG-File from the bq27510-G1 . According to the table 7 (Data Flash Summary) of the document "SLUS927-APRIL 2009", there are 3 values:
1. CC Gain
2. CC Delta
3. CC Offset
These values are floating numbers, But they are representated as hexwords on the data flash. I could read them out, but i have problems converting them back to floating numbers. I tried the IEEE 754 standard but it didnt work.
Can someone help me out pls? Its very urgent....
Thx in advance