Welcome to the Battery Management Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".
Q: Charging System of BQ24072 by 686746
Hi,
Now we set Riset=910 ohm; Rilm=1.1K ohm we found the thermal regulation
Should we lower charging currentby Riset as 1K ohm (890mA) as well as Rilm=1.6K ohm
or just lower current by Riset as 1K ohm (890mA)?
If the system consume under 110mA, charging current will keep as 890mA;
if the system consume over 110mA (i.e. 300mA), charger will enable DPPM mode, then draw 190mA from battery, right?
Regards,
Jose