ILIM setting in USB Suspend mode - BQ24075

Q: ILIM setting in USB Suspend mode - BQ24075 by 1120591

What is the current limit of the BQ24075 charger in USB Suspend mode. 

Specifically, when EN1 = EN2 = HIGH on the BQ24075, and it's in USB Suspend mode.   What is the ILIM (input current limit) setting in that case? Zero?

 

A: Re: ILIM setting in USB Suspend mode - BQ24075 by 96955

Putting the IC in suspend mode turns off the input FET so the ILIM is meaningless.  The ILIM pin typically applys only and adaptor mode since the input current limit is typically set above the USB thresholds.