hello, everybody:
I want to know, the UCD3138 can programed in CCS5.1?
if it's can used in CCS5.1, how can I set the configure in CCS5.1?
thanks first!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello, everybody:
I want to know, the UCD3138 can programed in CCS5.1?
if it's can used in CCS5.1, how can I set the configure in CCS5.1?
thanks first!
Hi you lee1,
We have a manual that can be used to convert a CCS 3.3 project to a CCS 5.2 project. We are also working on a tool that can convert automatically CCS 3.3 projects. The manual is available here http://www.ti.com/product/ucd3138 under the application notes section.
Thanks,
Sanatan
Hi Sanatan
But we don't have CCS 3.3. Only CCS 5.3 could be downloaded from TI website. It seems missing something for the starting. Don't know how to start with the writing the code for UCD3138 in CCS 5.3. CCS 3.3 is quite different to the CCS 5.3. Do you recommend any application note or manual that i could read for CCS 5.3 at the starting?
Thanks
Tom
Tom,
We don't have any information yet on beginning a project using CCSv5 or above. We usually start with code that has been written in CCSv3.3 and convert the project using the manual that Sanatan mentioned. The reason for this is because we will send out our EVM source code which was created in CCSv3.3 and use the manual to convert the project to CCSv5 or above. Thanks.
Regards,
Brandon Vonk
Hi Brandon Vonk
Could you please sent me the source code of interleaving control and phase shift control? We have bought two UCD3138OL64EVM-031 and UCD3138064EVM-166. On the other hand, could you please send me CCSv3.3 as well do that I could follow the document and application while programming? My email address is tomki_99@hotmail.com
Thanks
Best Regards
Tom
Tom,
I just sent you an email about this. You mentioned the UCD3138OL64EVM-031 and UCD3138064EVM-166. Those EVMs do not have code on them. They are for testing the UCD3138/UCD3138064 device itself, and/or/with the code that you create. Our other EVMs contain power stage boards that utilize a specific topology (PFC | LLC | HSFB | PSFB). Those EVMs contain code pre-loaded on the UCD3138 device, and that is what when we can send out the code.
Can you clarify what you mean by interleaving control and phase shift control? Which topology? Do you mean that you want the source code for the UCD3138PFCEVM-026, and the UCD3138PSFBEVM-027? Please clarify. Thanks!
Regards,
Brandon Vonk
Hi Brandon
Thanks for your email. Yes, I would like to have the code of PFC interleaving control and phase-shifted full-bridge DC-DC power conversion to begin with. My project is trying to migrate them into a single UCD3184064. It is hard to start from zero. It would be grateful if you could send me the codes so that I could learn/understand how the code work and how to design for my application.
By the way, do you have CCSV3.3 that could send to me? It would be very helpful as all the application notes/document/code written based on CCSV3.3 rather than CCSv5.5.
Thanks. I look forward to receiving your feedback shortly.
Best Regards
Tom
Hi Brandon
I have downloaded the UCD3138 CCS Template and tried to convert the code to CCSV5.5, which I have downloaded, following the manual. However, the error window prompted out with " #1559 Interrupt handlers must be compiled in ARM mode". I have no idea how to solve it. Does it work in CCSV5.5? Have you tried it before?
Thanks Tom
Tom,
Thanks for your questions. I have sent you an email with the source code and command files for UCD3138064 attached. In your latest email, you mentioned that you were using CCSv3.3. Is this still the case? If so, you will not need to perform this conversion, as the code was originally written in CCSv3.3. Please let me know. Thanks!
Regards,
Brandon Vonk