Hello there,
I am evaluating the power management on C6657 EVM platform. I noticed that the IinMon pin of the UCD9222 is connected to the MCP9700AT temperature sensor output.
Does this mean the input current monitoring should be disabled and this pin is sampling the additional external temperature(this pin is used as Auxiliary ADC input 4 rather than input current monitoring)? The multimeter reads temperature sensor output at 890mv(with 470mv offset,10mv/c step), which indicates that the additional external temperature is 42c.
Now in Fusion GUI, Iin(when checked) consistently plotting 0A, while the external temperature is showing the temperature sampled from the UCD7242.
So, how to configure in the GUI to display the additional temperature which is sensed by the MCP9700AT?
I appreciate for your kind help!
Best regards,
Jeff