Hello,
I am trying to use the UCD3138 and run the sample code and training labs that accompany the UCD3138PFCEVM-026 and the UCD3138CC64EVM-030. I have access to both CCSv5.2 and CCSv6, but no access to CCSv3.3, which is what all the template files were written in. I have attempted both the legacy import feature of the new CCS, as well as the migration template from 3.3 to 5.2, listed on the ucd3138 page.
It appears that I need access to the ccsv3.3 libraries or other tools generated by the older version of CCS before I can use the code with CCSv5.2 or later.
Has anybody had luck working with the template code or the training files in CCS5.2 or later without having access to CCSv3.3? Were there any missing library files, linker errors, or other issues? How did you overcome these? Furthermore, does anybody have working UCD3138 template files for CCS5.2 or later?
Thank you for the support.
Best,
Keenan