Hi I have been working with Xilinx FPGA kintex 705. This board has 3 ucd9248. One of them on rail 4 stop working and I cannot fixed. I hope with your support I can solve the problem.
If you want to take a look on the schematics here is the link:
https://casper.berkeley.edu/wiki/images/1/10/Kc705_Schematic.pdf
I have problems with U55, address 52. The fault signal FTL happen and then there are no output on PTD08A010 because the SRE-4A signal on pin 33 is always down.
I try to follow the suggestion on this post:
http://e2e.ti.com/support/power_management/digital_power/f/184/p/114400/415673.aspx#415673
by Mark Hagen : "Unfortunately, the FLT indication from the driver/power module does not have a corresponding fault response command. So the recovery must be handled by the host by either sending an OPERATION command to turn off, then on, or by cycling the PMBus CTRL signal."
But still the problem continue.
I appreciate to much your help to solve this issue.
Best,
Marcelo