This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Sebastien,
We are moving these source codes through our legal process to get approval for proper customer distribution. I apologize for the extended wait. The EVM ships with firmware already loaded onto the device for introductory purposes of evaluating the hardware during initial design process. Are you able to run the PSFB EVM with the firmware that was included with it? Have you taken a look at the Training Codes yet?
I'll get back to you as soon as the process has finished and we have received approval for proper source code distribution. Again, I apologize for the wait.
Brandon,
>Are you able to run the PSFB EVM with the firmware that was included with it? Have you taken a look at the Training Codes yet?
Yes I started with Training Codes from TI and I continued with EVM. Today, I have designed my own module and I think this component is promising. In this module I have implement voltage mode but for current mode with analog peak current mode on front end 2 I have more difficulties . That is why I would like some examples from EVM to do that.
In programmer's manual you say :
Refer to the reference firmware code provided with UCD3138PSFBEVM-027 and TI application note for Phase Shift Full Bridge peak current mode control implementation with UCD3138.
I have this EVM and no source code was included with it. I'll wait....
>I'll get back to you as soon as the process has finished and we have received approval for proper source code distribution. Again, I apologize for the wait.
OK.