Hi,
I am using UCD9222 (2 Qty) and UCD9244 (1 Qty) in our board.
For my application, i have given +12V source to UCD9222 and UCD9244. It is working good. Here, the +12V is generated from the backplane and rise time of +12V source is 35Micro Seconds (us). In this condition, this PWM controller's are working good as per my program.
Then, I have connected +5V source to UCD9222. Here, the +5V is generated from the backplane and rise time of +5V source is 25Micro Seconds (us). Compare to +12V source, it is taking less time to give 5V from the backplane. In this condition, my PWM controller is not giving the output voltage from the module. When i put this card in different backplane, same this 5V section of PWM controller is not working. But, at same condition, +12V PWM controllers are working good. The difference of both the source is 12V having rising time of 35us and 5V having rising time of 25us.
Can you clarify whether any settling time is required for the UCD controllers when connected to 5V?
Regards,
MagalingamVisio-Rampup signal.pdf