This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD74106 no load offset accuracy ?

Other Parts Discussed in Thread: UCD74106, UCD9246

Hello,

I'm using UCD74106 and I've got some important variations from one board to another on current measurement.

5% tolerance on the internal current measurement + 5% error gain + 1% external resistor + 10mA of INL at UCD9246 ADC, I was expected some decent accuracy.

With current of 0.5A, I sometimes read 0.25A, sometimes 0.75A (on different boards but exact same hardware)

I suspect the "Zero amp load offset", in the datasheet, only a typical value is provided, could you give me an estimated min/max ?

Thank you,

Thomas