The datasheet title for TPS51604 is "Synchronous Buck FET Driver". I would like to use it in a boost application.
Nothing in the function block diagram jumps out at me.
Does anyone see anything that might prevent it from being used?
My application is to boost a ~3.7V battery to 24V (30 watts max) and I do have 5V available to power the driver. My Switching freq is 500k to 1MHz so its adaptive near zero dead time reducing Qrr losses is very nice!
Thank you,
Chris