Hello,
I have an issue with the UCD9222 not enabling the DSP(C6655) core voltage. I connected the USB pod to use the Fusion software to see what might be wrong and as soon as it sees the device the device starts to work? I unplug the pod and power cycle and I am back to a nonfunctioning board. I probe the PMBUS_CNTRL line and it is high which should enable the part. Any ideas?
Another question, the UCD3000 Gui will recognize the device which according to the link below means the firmware is intact? What would cause the firmware to be corrupted?
http://e2e.ti.com/support/power_management/digital_power/f/184/p/188586/677844