Hi,
I am using CCS6.1 to develop firmware for UCD3138. As the UCD3138 sample code suggest, I chose the device as " generic ARM 7" instead of "UCD3138", but when I use spectrum digital XDS510 to connect the target, for the device available I have only UCD3138 to choose. I am not sure this is the reason, but when I try to load the firmware, I always got the error " Does not match the target endianness" . I have attached the screen capture for your reference.
Thanks,