Hi All,
I'm working with UCD3138064 40 PIN QFN Device.
Referring to the Datasheet SLUSB72B (UCD3138064.pdf), I've noticed that there are two different Tables in Chapter 3, with conflicting values: I'm talking about Flash Memory (Program).
Referring to the Table 3.1 - Device Comparison Table, i can see a value of 64KB for this MCU.
Referring to the Table 3.2 - Product Selection Matrix, this value changes along with the number of PIN, in my case the values is 32KB. (As you can see below)
I would like to know if the MCU has 32KB or 64KB as Flash Memory (Program) size. Is it possible that the second Program Bank (Bank2) is unavailable for this MCU with 40PIN?
Thank you for you reply.
Best Regards,
Massimo