This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using UCD3138CC64EVM-030 to follow the training material of the UCD3040 tutorial course

Other Parts Discussed in Thread: UCD3138, UCD3138CC64EVM-030, UCD3040, UCD3138064

Training 01 - Hello World - Solution.rarHello

I have UCD3138CC64EVM-030 and the UCD3040 tutorial training course material. I followed the training course Lab1 to learn the UART of the UCD3138 to communicate to PC hyperterimal to show "Hello world!". Firstly, I compared the source code, head file, linking cmd and data sheet of the UCD3138 with UCD 3040. There are almost the same function except additional  functions of the UCD3138. I use CSC3.3 and USB fusion tool to compile and download the train0.x0 to EVM without any problems. Unfortunately, I still can not get the results of this training course 1 to show "hello world" on the PC screen. What I did are summary as follow:

(1)UART

 UCD3040 --SCI-TX                              UCD3138 -SCI-TX0    

                      SCI-RX                                                 -SCI-RX0

                                                                                      -SCI-TX1

                                                                                     -SCI-RX1

The training note only wrote to connect RS232 to UCD3040. I check UCD3040 has a UART but UCD3138 has two UARTs. I have try two UARTs of UCD3138. However, the hyperterminal shows nothing.

(2)I use a USB to RS232 adapter(GMUS-03) and operate at Win XP system. I am thinking that should I do an extra circuits of RS232 to connect UCD3138 UART? like HN232 IC??? I can not find any circuit description of the UCD3040 about this.

(3)The source code is read only in the CSC3.3 environment . That means the code can not modify and these codes come from TI.

Can you help me to finish this training course by self learning? I upload the training course in a zip file.