Hello!
We use two UCD9244 + 2 x UCD7242 in our project for Zync7000 FPGA supply.
We have two problems:
1. How to program UCD9244 Power Good pin #24 by means of Fusion Digital Power Design? Power Good line pull-ups to Vdd (3,3V) in our desing by 10kOhm resistor. Power Good is set low when UCD9244 overheat. Power Good is set to Hi-Z when all power rails is ok. May I change Power Good pin Hi-Z state to only High state? How can I do it?
2. We use Fusion Digital Power Design (version 2.0.120) for UCD9244 configuration. I read in UCD9244 datasheet (page 21): Additionally, the UCD9244 has three banks of filter coefficients: Bank-0 is used during the soft start/stop ramp or tracking; Bank-1 is used while in regulation mode; and Bank-2 is used when the measured output current is below the configured light load threshold. How I can program bank 2? Why bank 2 tab is absent in Fusion Digital Power Design?