Hello,
it might be a very simple question, but I can't find the answer.
I have FAULT_MUX interrupts set as FIQ.
I have AcompB set for threshold and polarity, but ACOMP_B_INT_EN is set to 0
The fast interrupt routine happens when the voltage on the comp B pin is above the threshold. How does this happen if the interrupt is disabled? I have also verified on memory debugger that ACOMP_B_INT_EN is not set.
Are all fault interrups enabled globally somewhere in the code (this is a modified version of the EVM code)?
What is the purpose of ACOMP_B_INT_EN if the interrupt is triggered anyway?
Thank you