Hello.
I have questions UCC3138.
1 Please let me know the maximum parallel operation in each mode such as average current mode,
master slave mode etc.
Is it possible to operate 12 units in parallel?
2 In average current mode, one unit operating in parallel will fail.
In this case, it seems that it can operate normally if the share bus is connected.
Is this idea correct?
3 I want to realize parallel operation and redundant operation.
In this case, I think that master slave mode is the best.
Is it OK?
4 Do I need to consider the total capacitance( total capacity on the circuit) on the external capacitor capacitor?
For example, 0.033 uF for one. 0.099 uF when 3 units in parallel, 0.396 uF in 12 units in parallel.
Is this way of thinking OK?
thank ypu.