Hi all,
I have some questions about analog comparators.
1. For 64 pin UCD3138, in pin #5 which is AD07, it's written as "Connected to comparator F and reference to comparator G". In this explanation, "reference to comparator G" statement is not so clear for me. Can you please make this a little bit more clear
2. Pin #8 which is AD03 is connected both comparator B and C. Does this mean that comparator B and C can not be used independently? As far as I understood, only one measured value such as output voltage, can be connected to AD03 and if I enable both comparator B and C, they both compare the measured value (Vout) with the corresponding reference values. If this is the case, what is the main purpose of placing two comparators in a pin?
I would be appreciated if someone helps me.
Kind regards,
Steve