Hello, I have recently learned UCD3138 full bridge hard switch development board source code.
I would like to ask two questions.
The first question: why the function “void swi_single_entry (Uint32 arg1, Uint32 arg2, Uint32 arg3, Uint8 swi_number) ”and function “void software_interrupt (Uint32 arg1, Uint32 arg2, Uint32 arg3, Uint8 swi_number) function” name is not the same, but the content can be mutually transfer?
The second question: MiscAnalogRegs.CSTRIM.bit.RESISTOR_TRIM = 23; I can not find a detailed description of the register CSTRIM in the manual, where can I find?
thanks.