This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD3138A: UCD3138ARMHR adc sampling error

Part Number: UCD3138A

Dear TI,

We found a UCD3138ARMHR failed to accurate adc sampling.The fail IC can not correctly read the ADC input voltage when the adc voltage below 1V.

Test condiction : the DC Source value directly connect to adc,and we read ADC value in register.

The tabel bellow is ADC test data result : the voltage input and read  are not same.

Can you explain  it, is the chip had broken?

Best Wishes

LEI