Hi,
I met a problem when testing UCD3138A64OEVM-662: the firmware "Lab_2_UCD3138A64.x0" cannot be downloaded into the EVM.
After I launched "UCD3XXX Device GUI" and click on "Scan device in ROM mode", it seems the GUI has identified the device:
After I donwloaded the firmware it shows the firmware "Download completed without error...":
Whereas I found the firmware did not execute at all after download. And it says "No devices found" when I click on "Command ROM to execute its program":
Actually it is ensure there is no any problem with the connection between GUI and EVM since I can configure the device to output PWM signal through memory debugger. I am not sure what is wrong?
Could you please help me with this problem?
Thank you,
John