Dear all,
I am working on Digital power Buck converter using C2000 series controller. I have used Digital power kit as reference. The controller is C28035.
Now i have build my own hardware, it is running at frequency of 50KHz, as the power is too high. it is 450W.
Situation: I have seen Buck converter in kit, and Coefficient B2, B1, B0, A2, A1 in code.
Question: How they are calculated? Or How to calculate the resistance and capacitor values for buck type 2 feedback?
My Knowledge: I have converted the analog resistor capacitor to B2, B1.... coefficient using Discrete conversation. I have the formulas, and knowledge, how it is done.
Now as the components are known of kit, i cannot verify the coefficient values.
I wants to verify that the procedure of calculating the feedback component is same. Can you give me a refference to calculate Type 2 compensation for Buck also.
Vikas Dabas
India