Dear lan,
I have a question about Non Linear PID for Hard-Switching Full-Bridge DC-DC Converter, the frequent is 174kHz.
Programmable Non-Linear Limits for automated modification of filter coefficients, The max cross-over frequency is 5.6kHz.
When do output dynamic test, within a period the Duty reduced from 40% to 10%.
I wonder whether the dynamic trigger the fastest PID coefficients,the fastest PID can adjust the duty ratio quickly within a cycle? I don't understand the loop can be adjusted so fast., just one period. can you give me some opinion?
I also want to know in detail how to switch PID coefficients according Non-Linear Limit in UCD3138A? For example, change KP ,KI , KD in turn or modify the KP ,KI , KD as a whole?
Whether the way of change PID will affect dynamic response?
Best Wishes
LEI