Other Parts Discussed in Thread: UCD9248, , TPS51116
Hi,
my circuit is composed of a power controller (UCD9248) and a PowerTrain module (PTD08D210W).
The output voltage of the PowerTrain modules is used as the termination voltage of our electronic component.
I have some questions
Q1: can the PowerTrain module PTD08D210W as source/sink be configured?
Q2: if the sink mode is possible.
- what values are valid in the Isense output (PTD08D210W) when the output current is negative (Sink mode)?
- which parameters must be configured in UCD9248PFC with FUSION_DIGITAL_POWER_DESIGNER
Regards,
Oscar.