Hello! I want to use the CNTL_2P2Z.asm block (from digital power lib) as PI controller for a PFC application. The constants in the controller can be calculated as in the figure below (from TI's 2p2z PID derivation). KD' will be zero in my case (PI-control).
My concern is that KI' will be very small if the sampling frequency is high, is that correct? If I am performing ADC from sensors with 100 kHz frequency, then KI' will be KI*(10^-5)/2. Therefore b0 and b1 will pretty much equal Kp' and -Kp' respectively. Will that not remove the influence of the integral part?
Am I thinking about this incorrectly? Thankful for answers!