Hello, I'm learning about the UCD3138's hard-switched full-bridge firmware.
I have some problems with void init_loop_mux(void){}.
Void init_loop_mux(void)
{
LoopMuxRegs.FECTRL0MUX.bit.DPWM0_FRAME_SYNC_EN = 1;
LoopMuxRegs.FECTRL2MUX.bit.DPWM1_FRAME_SYNC_EN = 1;
LoopMuxRegs.FECTRL1MUX.bit.DPWM2_FRAME_SYNC_EN = 1;
}
I know that the above program synchronizes a certain PWM frame to a front end,
but I don't know exactly what frame synchronization means. Is frequency synchronization or simultaneous activation?